Part Number: NE555
Other Parts Discussed in Thread: SN74LVC1G123
Tool/software:
I want to use logic circuit to act as power button on a PC.
The PC is not accessible when DC power is applied to the motherboard and can not access the button to power up the system.
I tied using the attached file.
But, the 555 timer stays on since PIN 2 (Trigger) is held low and timer does not expire after 5 seconds or so.
The Power GOOD from 5VDC supply suppose to trigger the 555 time and the PIN 3 output is inverted and sends a low signal for 5 seconds to power up the motherboard.
I need a better solution.
Thank you