Part Number: LMK00105
Tool/software:
Hi Team,
This is FAE Jayden, My customer has some questions about the VDD pin (Pin 23 and Pin 8):
- Are these two pins (Pin23 & Pin8 ) are internally connected together?
- As customer will use 4.75k pull-up resistor to connect pin23 to 3.3V,so there is a 0.15V voltage drop on Pin 23; And Pin 8 is connected to 3.3V directly; Is it okay for ZTE's design as there is voltage difference between these two pins?
Brs
Jayden