Part Number: LMX2820
Tool/software:
HI!
After the LMX2820 instant calibration initialization, the frequency was changed from 5.65GHz to 10GHz. The LD lock time is 6 seconds. Procedure
Without power off, 10GHz lock off after even calibration:
R1:0X57A0
R0:0X6430
R0:0X6420
At this point change the frequency to 8GHz and then turn even calibration on again:
R1:0X57A1
R0:0X6430
R0:0X6420
The LD lock time is 82ms.
Please ask why the locking time required for instant calibration is so long in this case.
Can I shorten the lock time?