This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B12204: LMK5B12205 supply

Part Number: LMK5B12204


Tool/software:

Hi TI Team!

for device LMK5B12204, the planned output formats are:
OUT0: LVDS (differential)
OUT1: 1,8V LVCMOS (single ended)
OUT2: 1,8V LVCMOS (single ended)
OUT3: 1,8V LVCMOS (single ended)

I have two questions please with focus on the application mentioned above:
1) Is it sufficient to supply all VDDO_0/1/2/3 each with 1,8V?
2) Is it allowed to supply all VDDO_0/1/2/3 each with 3,3V?

Thanks,
Martin

  • Hi Martin,

    1. For the above format list, all VDDO supplies can be configured as 1.8V.
    2. For the above format list, all the VDDO supplies can be configured as 3.3V too; however, the LVCMOS outputs (per note 2 of the datasheet image below) will not be exactly 1.8V (will be a bit higher, around 2V due to the LDO drop out voltage). If 1.8V LVCMOS output is desired, I recommend routing 1.8V to either all supplies or just VDDO_1, VDDO_2, and VDDO_3.

    Regards,

    Jennifer