Tool/software:
Hi Team,
TI CC13x2/26xx/CC2340 need 48MHx XTAL.
Please help to check if LMK6CE04800DDLFR can be used for CC13x2/26xx/CC2340 as 48MHx XTAL.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mike,
LMK6C is a crystal oscillator (XO) not a XTAL - this means the XTAL driver oscillator circuit is already built in the device.
Can you share the reference clock requirements?
Does it have to be a XTAL input?
I found this online but rather confirm and be sure.
I would check with the CC13x2 team and ask about the input stage - can we use an XO or does it strictly need to be a XTAL?
If the answer is we need to use a XTAL then unfortunately LMK6C is not an option.
The reason I ask you to check with the other team is due to this statement.
It seems certain family of this device does allow for an XO clk input instead of XTAL.
Best regards,
Vicente