This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1108: Provided IBIS model not working in Altium

Part Number: LMK1C1108


Tool/software:

Hello, the only forum I can place this in is "clock & timing forum", but this issue is about the IBIS model (LMK1C1108 data sheet, product information and support | TI.com)

The .ibs model I downloaded (SNAM243.ZIP) for LMK1C1108 is unable to be inserted into my Altium Designer 22 as an Ibis model.

The error:

Running on Altium Designer 22, the Altium documentation states "This feature supports all versions of IBIS model specification, up to and including version 4.0" - https://www.altium.com/documentation/altium-designer/ibis-model-editor?version=22

When reading the lmk1c1108.ibs file, the IBIS version is 1.0
I am also unable to use the ibischk7 program to check if the .ibs file is correct because the program only checks "IBIS specification from IBIS 2.0 through IBIS 7.2" - https://ibis.org/ibischk7/

Any recommendations or fixes?