This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM7005: Inquiry about use case

Guru 11480 points
Part Number: CDCM7005
Other Parts Discussed in Thread: LMK04828, LMK04832

Tool/software:

Hello,

My customer wants to use CDCM7005 under the following conditions. Is it possible?

   - VCXO_IN = 122.88MHz / PRI_REF = 1 PPS(GPS/IEEE1588) / Output Clock = 30.72MHz

Thank you.

JH

  • Hi JH,
    Yes,
    We can utilize a R divider of 25 & and N divider value of 3072 to achieve a 0.04MHz PFD which should achieve lock. 
    Please note detection circuitry is unavailable at a frequency this low according to note in DS. 

    Please note a newer better performing jitter cleaner such as LMK04828 or LMK04832 can perform this function as well. 

    CDCM7005 is a cheaper alternative as the cost of phase noise. CDCM7005 is also not supported in PLLatinumSim where as LMK0482x family is. 

    Best Regards, 

    Vicente