This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334: Power save

Part Number: LMK00334

Tool/software:

Hi,

Can I leave VCCOB and VCCOC floating to save power when CLKOUTB and REFOUT are not used on the board?

Regards,

Wei

  • Hi Wei,

    It is not recommended to leave VCCOB and VCCOC floating to save power. When CLKOUTB and REFOUT are not used on the board, the recommended way to save power is to leave each of the associated outputs floating, or disable them if possible. It is not possible to enable Bank A and disable Bank B, so the best route of action is to leave the outputs from Bank B floating, and to disable REFOUT.

    Thanks,

    Michael