Part Number: LMX2594
Tool/software:
Hi,
I have a few questions regarding the differential output:
- Can I use a differential output directly without converting it to single-ended.
Purpose: To provide a sampling clock for a DAC.
Sampling Frequency: 12 GHz
The DAC requires a differential sampling frequency input. Instead of using a balun, can I directly connect the LMX2594 differential output to the DAC?
-
If it is possible, can you share the circuit configuration?
-
What would be the output power level when using differential mode?