Part Number: CDCE913
Other Parts Discussed in Thread: CDCE949
Tool/software:
Hi all,
the CDCE913 internal load capacitors are programmable from 1pF to 20pF via register XCSEL.
Question: is this the capacitance per capacitor, or is it the resulting load capacitance (CL1 in series with CL2)?
I read "Practical Consideration on Choosing a Crystal for CDCE(L)9xx Family" (SLEA071) and "VCXO Application Guideline for CDCE(L)9xx Family" (SCAA085A).
I think it's per capacitor, but am not absoutely sure.
So to get effective 10pF load capacitance for the crystal I would program 16 pF (XCSEL = 10h), correct?

With CL1external = 2pF, CL2external = 6 pF and CL1internal = CL2internal = 16 pF we get:
CL1 = (16 + 2) pF, CL2 = (16 + 6) pF and thus CL = (18 x 22) / (18 + 22) pF = 9.9 pF
Correct?
Regards,
Wolfgang