Tool/software:
I want to create a 60Hz pulse signal using an ultra-low power consumption IC.
In the following thread, in response to a question about creating a 20-40Hz pulse signal, the answer was that it can be done with TPL5010.
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/991956/pulse-signal-generator
However, the datasheet states that you can only select intervals from 100ms (10Hz) to 7200s (0.000138Hz).
Specifically, how can we create a 16ms (60Hz) pulse signal?