Part Number: LMX2592
Tool/software:
Hello,
I am using the lmx2592 and I am using a 100 MHz external reference clock.
I am using the doubler to increase the the pfd to 200 MHz.
I have attached the registers I am writing in the file registers.txt.
However it is only locking for certain frequencies. 2Ghz and 6.4GHz are working for example but 6GHz is not working.
If I am not using the doubler and use 100 MHz pfd everything works fine and the lmx2592 locks.
R70 0x460116 R69 0x450064 R68 0x4407BC R67 0x4371FD R66 0x420002 R65 0x412800 R64 0x400077 R63 0x3F0094 R62 0x3E0000 R61 0x3D0001 R60 0x3C0000 R59 0x3B0000 R58 0x3A0000 R57 0x390000 R56 0x380001 R55 0x370000 R54 0x360820 R53 0x350080 R52 0x340000 R51 0x334180 R50 0x320300 R49 0x310300 R48 0x3003FC R47 0x2F08CE R46 0x2E08A3 R45 0x2D0000 R44 0x2C0000 R43 0x2B0000 R42 0x2A0000 R41 0x2903E8 R40 0x280000 R39 0x278204 R38 0x26001E R37 0x250000 R36 0x240000 R35 0x230019 R34 0x22C3EA R33 0x212A0A R32 0x20210A R31 0x1F0401 R30 0x1E0034 R29 0x1D0084 R28 0x1C2924 R27 0x1B071A R26 0x1A027C R25 0x190000 R24 0x180509 R23 0x178842 R22 0x162300 R21 0x150064 R20 0x14012C R19 0x130965 R18 0x1203C0 R17 0x11E114 R16 0x100037 R15 0x0F0025 R14 0x0E0CE7 R13 0x0D4000 R12 0x0C7001 R11 0x0B0018 R10 0x0A10D8 R9 0x090B02 R8 0x081084 R7 0x0728B2 R6 0x06C802 R5 0x0500C8 R4 0x041943 R3 0x031902 R2 0x020500 R1 0x010808 R0 0x002118