Other Parts Discussed in Thread: LMK5B33216, LMK5C33216A, LMK5B12204
Tool/software:
Hello,
I want the LMK05318B to output a clock synchronized to a 1PPS reference input.
I was able to configure it in TICS PRO, and the DPLL locked onto the 1PPS reference, giving me a 1PPS or 25Hz output on out7, but there is a phase offset between these outputs and the rising edge of the reference.
I tried to use ZDM to deal with the phase offset, but the ZDM item in TICS Pro has been deleted and can't be found.
So I tried writing 1 to the DPLL_ZDM_SYNC_EN bit of R252 in the Raw registers section and checking CH7_SYNC_EN in the Outputs section, but the phase offset was not resolved.
How can I enable ZDM for LMK05318B in TICS PRO 1.7.7.6?
Regards.
Takaya