Part Number: LMX2594
Tool/software:
Hi TI,
I am using clock 104 module on the rfsocZCU208 board.
- Configured the lmx2594 for 1966.08 MHz
- Ref clock for lmx is from lmk04828b and frequency is 245.76MHz.
- Frequency of PFD is 245.76MHz.
- N divider value is 48.
- Osc2x is disabled and pll_R and pll_Rpre divider values are 1.
- Vco frequency is 11796.48MHz.
- Channel divider enabled for both rf out A and out B.
- Measurement of clock frequency from out B port(SMMP to SMA converter used) on Keysiggt MXA signal analyser.
- Verified the R25 value for 0x0c2B.
- Reduced the CP current at R14 register
Any suggestions what went wrong in this case??
Thanks
Raagu