Dear all,
I would like to point out that we have observed a non-constant skew of the CDCE62005 after a SYNC.
In this post skew refers to the phase between the CDCE62005 input clock (its reference clock) and its output clock(s).
In our application a constant skew is mandatory and we have chosen the CDCE62005 because of its capacity to synchronise the output dividers with the reference clock using the SYNC signal.
Concerning the SYNC signal we have used the following setting:
R4.1=1 (“outputs have deterministic delay relative to low-to-high pulse of SYNC pin when the SYNC
signal is synchronized with the reference input”).
R6.20=0 (“when set to "0", outputs are synchronized to the reference input on the low-to-high pulse EEPROM on SYNC pin or bit”).
We have produced 25 boards using this component. Because we have found out this non-constant skew we have extensively tested these boards. The test consists in generating multiple SYNC sequences and measuring the skew on an oscilloscope. We have also observed ambient temperature dependency. Thus we have done this test for 2 different temperatures (10C & 35C). The number of cycles for each temperature was 500.
We have found 12 boards (thus 12 CDCE62005) with a non-conform behaviour (at least non-conform for our application). Indeed for these components the skew was changing between 2 different values separated by around 1ns (which corresponds to the clock period after the prescaler).
This variation happens on some boards very rarely (e.g. 2 times for 500 cycles) but on other boards much more frequently (e.g. 238 times for 500 cycles) and the phenomena depends on the ambient temperature. For some components it never happens (at least for 500 cycles) at 35C but we can observe the variation at 10C (but this is also right in the opposite direction for other components).
Could you tell us if this behaviour is normal and/or known by TI or do you have any clue of what we could have done wrong?
Cheers,
Stéphane