This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: Jitter on PLL Clock on status and shape of 1GHz output

Part Number: LMK03318
Other Parts Discussed in Thread: LMK00304, TRF1305B1

Tool/software:

Hi,

I am evaluating the LMK03318 using TI's EVM board. I measured the output waveforms on a Scope. I have a couple of questions:

  1. The 1 GHz output looks more like a sinewave. Is this the best that can be expected? If so, can you recommend a device that can clean this up downstream?
  2. When using the PLL clock from the status pin as a scope trigger, the waveforms are more jittery, indicating that the 3.3V output itself is jittery. I was thinking of using this output in my end application as a time base sync. But, looks like, I shouldn't use this. Would you concur?
  3. Why does the EVM have capacitors in-line on the clock outputs? For AC coupling? Could they be degrading the 1GHz waveform?

EVM CharacterizationForTI.pptx

Thanks,

Prasoon