This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214: Detail specification

Part Number: CDCE6214

Tool/software:

Hi team,

Could you provide the value, to the extend possible.

Average Clock Period Accuracy(Min~Max)[ppm]                                   
Absolute Period (including Jitter and Spread Spectrum modulation)(Min~Max)[ns]
Cycle to Cycle jitter(Max)[ps]
Peak Period Jitter(Max)[ps]
Jitter Phase Noise @500kHz(Max)[dBc/Hz]
Jitter Phase Noise @1MHz(Max)[dBc/Hz]
Frequency Tolerance(Min~Max)[ppm]
Max Deterministic Peak-to-Peak Jitter @10^(-6)BER(Max)[ps]
Peak Phase Jitter(Max)[ps]


Best regads,
Goto