This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572EVM: Max. achievable bandwidth in Automatic/Manual Ramping mode

Part Number: LMX2572EVM

Tool/software:

Hi Noel, 

Then what is the maximum achievable ramp bandwidth and could you please tell the parameters that determine it ?

Regards,

amrita

  • Hi Amrita,

    As shown in the datasheet, the slop is determined by RAMP_INC (in frequency) and phase detector frequency.

    This slope represents the capability of the ramp engine. Actual performance is limited by the loop bandwidth, higher slope requires wider loop bandwidth. 

  • I am sorry I am in the process of understanding the LMX board..so need some more clarification.



    Is delta f that is highlighted above related to the loop filter bandwidth and how do we set fTh ..what is it based off of?

    Thanks.

    Regards, 

    Amrita

  • Hi Amrita,

    Suppose you want the device to ramp 50MHz in 100µs and your fpd is 100MHz.

    Frequency will increment every fpd cycle, i.e. 0.01µs. 

    Your desired ramp time is 100µs, there are 100/0.01 = 10000 ramps. (RAMP_LEN)

    Each ramp will change 50M / 10000 = 5kHz (delta f)