Part Number: LMK00804B
Other Parts Discussed in Thread: LMK1C1104, LMK00304, LMK00334, LMK00804
Tool/software:
I am seeing an issue where noise is being injected on an input to the part, as well as the output becomes unusable/unstable.
With a 1Hz (1 PPS) input on both the LVCMOS and the DIFF input set up as a CMOS input, I see noise on all inputs and the output when the CLK_SEL is changed from a 1 to a 0.
When it is at a 1, both inputs look fine and the output follows the selected input. It is when I change the CLK_SEL to be a 0 that I see the issue,
What should I be looking towards to help determine why I am seeing this error. I also see this issue if I don't drive the LVCMOS input with any signal.
In attached pictures. Buffer input = LVCMOS input) Resistor Divider is the P half of the diff input. ZL_INPUT is the output of the LMK008804 PPS_CLK_SEL is the select input.