Part Number: CDCS503
Other Parts Discussed in Thread: CDCE913
Tool/software:
Hello,
I want to use the CDCS503 as a clock multiplier in my circuit.
From the datasheet, the minimum clock input frequency is 8MHz.
I would like to drive a CMOS clock input at 5MHz frequency, will the decive work properly?
Generally, can one exceed the 8MHz-27MHz input frequency range (lower frequencies) under a condition of high enough slew rate?
Thanks,
Ziv