This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B33216: TCS config file creation

Part Number: LMK5B33216

Tool/software:

Hi apps team,

One of my customers is asking for a .tcs config file with settings corresponding to the template below. Can we share this?

Inputs: (2) 1PPS inputs from different sources (pre-config’d. i.e. not live switching)

Output 1,2: jitter cleaned 1PPS

Output 3,4: disciplined 10MHz

Zero Delay Mode output relative to input: yes. Need zero delay between PPS output and input and 10MHz rising edge to be coincident with 1PPS

Best,

Camilo