Hello,
After reading carefully the datasheet of the LMK1C1108, twice, I still don't know if I can drive directly a 50 ohm transmission line (without series termination in the near end) and a 50 ohm parallel termination (in far end).
On the one side, page 5 of the DS indicates a typical Rout (output impedance) of 50 ohm for a 3.3V supply. So far so good. However, in the same page, it also indicates "VOH (Output high voltage) minimum 2.8V for a IOH of 1 mA, which implies a maximum Rout of 500 ohm! Can you, please, clarify this?
Best regards,
Jose Jimenez