This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: PLL2 DLD Edge falls

Part Number: LMK04828
Other Parts Discussed in Thread: ADC08DJ3200, ADC08DJ3200EVM, LMX2582,

Tool/software:

Hi everyone,

I have a design similar to the ADC08DJ3200EVM with an ADC08DJ3200, a LMK0828 and a LMX2582. The design works on a lot of the boards but doesn't work on a few of them. When I read back the registers on those chips, the only obvious change is the register 0x183 on the LMK that has the value 04 on the non working board instead of 0 on the working one. The register definition says that it means PLL2 DLD edge falls. I guess that mean the PLL is not stable and going in and out of lock, but what can I do to diagnose those board that don't work?

Regards,

Étienne Drouin

  • Hi Étienne,

    Would you be able to provide a schematic or block diagram? 

    As you stated, PLL2 has lost lock. The fact that PLL1 did not lose lock tells me that the input signal is valid and the XO is working. However, it is a bit concerning that PLL2 is not locking. Generally, that should be able to lock, even without a valid reference signal. Would it be possible for you to share the clock tree, as well as the configuration file for the LMK04828 (preferably as a .tcs file, but a hex file will also work).

    Thanks,

    Michael

  • Hi,

    We don't really use .tcs file. I used the ADC12DJxx00 GUI to configure everything and that gives a .cfg. I tried to create some hex files using TCIS pro, tell me if that help you. I don't really know what you are looking for when asking for a clocking tree, we have one clock going from the LMX to the LMK and one clock from the LMK going to the ADC.

    Étienne

    R0 (INIT)	0x000090
    R0	0x000080
    R2	0x000200
    R3	0x000306
    R4	0x0004D0
    R5	0x00055B
    R6	0x000600
    R12	0x000C51
    R13	0x000D04
    R256	0x010010
    R257	0x010155
    R258	0x010255
    R259	0x010300
    R260	0x010420
    R261	0x010500
    R262	0x0106F0
    R263	0x010711
    R264	0x010801
    R265	0x010955
    R266	0x010A55
    R267	0x010B00
    R268	0x010C22
    R269	0x010D00
    R270	0x010EF9
    R271	0x010F00
    R272	0x01100A
    R273	0x011155
    R274	0x011255
    R275	0x011300
    R276	0x011402
    R277	0x011500
    R278	0x0116F8
    R279	0x011700
    R280	0x01180A
    R281	0x011955
    R282	0x011A55
    R283	0x011B00
    R284	0x011C02
    R285	0x011D00
    R286	0x011EF8
    R287	0x011F00
    R288	0x012010
    R289	0x012155
    R290	0x012255
    R291	0x012300
    R292	0x012422
    R293	0x012500
    R294	0x0126F0
    R295	0x012701
    R296	0x01280A
    R297	0x012955
    R298	0x012A55
    R299	0x012B00
    R300	0x012C22
    R301	0x012D00
    R302	0x012EF0
    R303	0x012F05
    R304	0x013010
    R305	0x013155
    R306	0x013255
    R307	0x013300
    R308	0x013422
    R309	0x013500
    R310	0x0136F0
    R311	0x013701
    R312	0x013845
    R313	0x013903
    R314	0x013A00
    R315	0x013BA0
    R316	0x013C00
    R317	0x013D08
    R318	0x013E03
    R319	0x013F00
    R320	0x014000
    R321	0x014100
    R322	0x014208
    R323	0x014311
    R324	0x0144FF
    R325	0x014500
    R326	0x014618
    R327	0x014702
    R328	0x014802
    R329	0x014902
    R330	0x014A33
    R331	0x014B02
    R332	0x014C00
    R333	0x014D00
    R334	0x014E00
    R335	0x014F7F
    R336	0x015001
    R337	0x015102
    R338	0x015200
    R339	0x015300
    R340	0x01540C
    R341	0x015500
    R342	0x01560C
    R343	0x015700
    R344	0x015878
    R345	0x015900
    R346	0x015A78
    R347	0x015BD4
    R348	0x015C20
    R349	0x015D00
    R350	0x015E00
    R351	0x015F13
    R352	0x016000
    R353	0x016102
    R354	0x016244
    R355	0x016300
    R356	0x016400
    R357	0x01650C
    R369	0x0171AA
    R370	0x017202
    R380	0x017C15
    R381	0x017D33
    R358	0x016600
    R359	0x016700
    R360	0x016801
    R361	0x016959
    R362	0x016A20
    R363	0x016B00
    R364	0x016C00
    R365	0x016D00
    R366	0x016E04
    R371	0x017360
    R386	0x018200
    R387	0x018300
    R388	0x018400
    R389	0x018500
    R392	0x018800
    R393	0x018900
    R394	0x018A00
    R395	0x018B00
    R8189	0x1FFD00
    R8190	0x1FFE00
    R8191	0x1FFF53
    
    R70	0x460000
    R69	0x450000
    R68	0x440089
    R64	0x4000AF
    R62	0x3E0040
    R61	0x3D0001
    R59	0x3B0002
    R48	0x3003FC
    R47	0x2F00CF
    R46	0x2E0F37
    R45	0x2D0000
    R44	0x2C0000
    R43	0x2B0000
    R42	0x2A0000
    R41	0x2903E8
    R40	0x280000
    R39	0x278204
    R38	0x260040
    R37	0x254000
    R36	0x240C10
    R35	0x23019B
    R34	0x22C3F0
    R33	0x214210
    R32	0x204210
    R31	0x1F0601
    R30	0x1E0034
    R29	0x1D0084
    R28	0x1C2924
    R25	0x190000
    R24	0x180D09
    R23	0x178842
    R22	0x162300
    R20	0x140064
    R19	0x130965
    R14	0x0E018C
    R13	0x0D4000
    R12	0x0C7001
    R11	0x0B0018
    R10	0x0A10D8
    R9	0x090302
    R8	0x081084
    R7	0x0728B2
    R4	0x041943
    R2	0x020500
    R1	0x01080B
    R0	0x002218
    
    cfg_6400GSample_Jmode5_3.cfg

  • Hi Etienne, 
    We would need a high level block diagram or a schematic to better understand how these devices are connected. 

    How is STATUS_LD2 configured? If it's still configured as PLL2 lock detect this pin must be low. 
    As Michael mentioned normally PLL2 will always lock and the issue is usually PLL1. 
    Refer to this post for Mouser as to what we mean by a clock tree: https://www.mouser.com/pdfdocs/clock-tree-101-timing-basics.pdf?srsltid=AfmBOopPIP73EfPZf_orwc2hviFKawRamns5KmSmBptypqh_Iccs9osk

    Best regards, 

    Vicente 

  • Hi Etienne, 
    After reviewing your schematic, I have a better idea of how these devices are connected. 
    Given the reference comes from the LMX part - when the LMK04828 is unlocked do you know what the state of the reference clock is? 
    Is the LMX part also unlocked? 
    The LMX part outputs CML and is an open collector which requires an external pull up to VDD which you do have. 

    If you're 100% certain the LMX output clk being used as reference to LMK04828 is always valid - I would start suspecting the VCXO. 

    Best regards, 

    Vicente