Tool/software:
Hello,
I have LMK05318BEVM und it works very well.
How can I determine how much time it takes the generated output frequency to get locked (phase and frequency) to the input frequency?
For example, 1 KHz input (PRIREF_P) to 600 MHz (OUT4_P)?
For tow Modes:
1. DPLL Mode With Cascaded APLL2
2. DPLL Mode
In section SET DPLL in TICS Pro after runing the script i get: Total DPLL phase lock time ~= DPLL fastlock time + 2 * DPLL phase lock measurement time.
What is the DPLL phase lock measurment time?
BR
Zain