This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1983: Issues with PLL1 GenLocking

Part Number: LMH1983
Other Parts Discussed in Thread: LMH1981

Tool/software:

We are inputting NTSC to the LMH1983, only H Sync(15.75k) and V Sync(59.97) to achieve GenLock; we are not using F Sync. However when we read register 0x02, we are getting 0xE0. Which means PLL1 is not locked. Any ideas as to what may be the issue. Our 27MHz input is stable. We made sure that 0x05 has bits [4:3] set to Genlock and that 0x11 bits [5:4] are set to Never Align. We did notice that when we read 0x00, we are getting 0x84 and 0xC4. We are using LMH1981 Eval board to extract the sync pulses.