Hello,
For CDCE913:
- The device is featured as capable of either 2.5 or 3.3V output.
- Pin 6,7, VDDOUT can be 3.3 or 2.5V in "Terminal Functions".
- "RECOMMENDED OPERATING CONDITIONS" allows 2.3V to 3.6V range.
The question is that can I tie VDDOUT to 2.8V in order to get 2.8V output clock? It would be possible if 2.5V and 3.3V are lower and upper bounds so that [2.5, 3.3] is a range, but would be impossible if only these two power supply values can be accepted.
And does VO have the same voltage level as VDDOUT?
Could anyone help with this?
Tim Baker