Other Parts Discussed in Thread: LMK04828, LMK05318, LMK04832, LMK03318, CDCE6214
Tool/software:
Dear Technical Support Team,
I have been looking into the clock generator and jitter cleaner.
Input recovery clock from AMD FPGA SerDes.
Input clock (recovery clock): LVDS 100MHz
Output clock: LVDS 200MHz x2 (1 free-run output, 1 PLL output)
Q1.
Can LMK03328 input recovery clock ? It has not clean.
According to the following app note, it describes that narrow-loop bandwidth loop filter can clean jitter.
Can a clock generator act as a jitter cleaner?
Q2.
Do you have any recoomended clock device for clock generator an Jitter cleaner?
Required clock is only 2 output, so for example,LMK04828, LMK04832, LMK05318 seeems to be an over specification.
Best Regards,
ttd