Part Number: LMK04826
Tool/software:
Hi,
Here my system receiving the 10MHz (0-15dBm) reference clock from external source and by using i need to distribute as follows
2No's of 10MHz Output (40 dB isolation from output to the input port)
1No of 56MHz
4No's 10MHz for internal systems.
My requirement is without degrading the phase noise i need to distribute the signal to the sub systems as reference clock. And if external clock not present then i need to switch to the internal source. Even if the external signal coming with the over a wide range i need to provide the constant or fixed level to the internal sub module, is that possible. For Example, if the signal coming with low means received with 0dBm then it should accept my sub module bcz it accept only in the range of -2 to 7 dBm even if it coming with 15dBm also it should accept. Can i achieve with the LMK0482.
And if the VCO frequency of the LMK0482 is within the range of using frequency( For example, if the LMK0482 VCO frequency is 2.4G and i'm dealing with the s-band frequency does it effects the phase noise/ any spurious related problem.