Part Number: TPS62A02
Tool/software:
Hi,
For output discharge function, does there have any data in full temperture range?(ex. -40~125C)
Or maximum/minimum range? Thanks!

Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS62A02
Tool/software:
Hi,
For output discharge function, does there have any data in full temperture range?(ex. -40~125C)
Or maximum/minimum range? Thanks!

Jeff
Hi Jeff,
Thanks for using E2E.
We don't specify min/max for this parameter in general. But I have seen values between 68mA ...86mA over the full range. I hope this helps.
Best regards,
Sepp
Hi Josef,
You mean in both package? the DRL package typ is 60mA smaller than 68~86mA.
And is it related with temperture?
Thanks!
Jeff
Hi Jeff,
for the TPS62A02 (both packages) the second row (76mA) is valid only:

Best regards,
Sepp