Part Number: LMK05318B
Other Parts Discussed in Thread: LMK05318
Tool/software:
Hi Team
There are two questions need your confirm:
1. Customer want to use a external EEPROM for LMK05318B, because they can burn the external EEPROM before soldering. What is the required capacity of the external EEPROM? is 4KB enough?
2. The attachment is a firmware customer output. Please help check whether the configuration is correct.
XO input 25MHz
Output0/1: AC-LVPECL 156.25MHz
Output2/3: disable
Output4: HCSL 50MHz
Output5: HCSL 156.25MHz
Output6: AC-LVDS 156.25MHz
Output7: disable
Thanks