Part Number: LMK1D1208EVM
Tool/software:
Hi, we are evaluating the LMK1D1208EVM board, and we're experiencing some odd results, regarding the additive phase noise. in our configuration, we've added an TPS7A8900 before the LMK1D1208EVM, in order to filter the Power supply.
The clock source is in LVPECL format @100MHz, with the phase noise analysis :

in the other hand, all the outputs are loaded with 100Ohm differential load.
here is the phase noise analysis :
.
our concern is the two following points :
1) with the power supply filtered, and with the input as indicated above, the noise floor level is around -150dB where the datasheet indicated -164dB.
2) The additive phase noise is specified to ~60fs in specification, but in our case we can see an additive phase noise on ~200fs.
how can we explain these results ?
regards,
Yohann