Part Number: LMK5B33414EVM
Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hi TI experts,
When I connect the LMK5B33414EVM to the PC, the device manager does not show any new USB device, at the same time, TICSPRO and other USB2ANY software show that 0 USB2ANY interface can be detected, the following is the specific steps I do, could you help to see what's the wrong with my operations?
- Verify the EVM default jumper and DIP switch settings shown in manual
- Connect the 12-V external power DC power supply (1-A limit) to VIN4 and GND
- I didn't connect the reference clock because I don't have a signal generator on hand right now
- Connect the USB cable to PC, the USB light on the board is on, but TICSPRO shows "Detected 0 USB2ANY interfaces". Meanwhile there is no new USB device in windows device manager.
- Tried different PCs, including Win10, Win11, desktops and laptops, and have replaced the USB cable, but there is no change in the phenomenon.
- Tried updating the MSP430 firmware, but the firmware loader can't detect USB2ANY interfaces either.
Best,
Gaofeng