This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMKDB1102: Abs max rating of VDD

Part Number: LMKDB1102

Tool/software:

Hello team,

The abs max rating of VDD is 3.63V and recommended rating is 3.6V.
There are only 0.03V margin between abs max and recommended rating.
Is the margin really this small?

Best Regards,
Kei Kuwahara

  • Kuwahara-san,

    The absolute maximum is being specified as VDD + 10% - so 3.3V + 3.3V * 0.1 = 3.63V. The device can support operating voltages of 1.8V and 3.3V, so 3.63V as an absolute maximum voltage rating might seem a bit conservative, and the margin might seem small, but you must consider the width of the operating range. For the sake of the device, the supply voltage should be kept at 3.63V or less.

    Thanks,

    Michael