Part Number: LMK04832-SP
Other Parts Discussed in Thread: LMK04832, LMK04828
Tool/software:
Hello,
We're interfacing the CLKOUT to FIN1 or CLKIN of an LMK04832 to LMK04832 at 960MHz. We chose to make this interface LVPECL (Fig. 9-2). Hyperlynx simulations show that the Pull-Down Resistors work better at 75Ω and below. Is it okay to use a lower value resistor than the 240Ω as shown in the app notes? If so, how low can we go?
Thanks,