Part Number: LMK05318B
Other Parts Discussed in Thread: LMK05318
Tool/software:
Dear Experts,
At present, we are working on a local area network application that requires multiple LMK05318Bs to output clock signals of the same phase. Currently, we need to output a clock signal of 12.5MHz, and the XO crystal oscillator uses 24MHz. We have tested that there is a phase difference between the clock outputs of two chips after PTP calibration of the PRIREF input and 1PPS input; We would like to know if LMK05318B can achieve multi chip output phase synchronization and how to configure it. Thank you~