Part Number: LMK5B33216EVM
Other Parts Discussed in Thread: LMK5B33414, LMK5B33414EVM
Tool/software:
Hi Clock team,
I'm trying to program the EEPROM of the LMK5B33414 so that the OUT12 outputs a 0.5M clock on power up without configuration, but I seem to be running into a bug, as follows:
I need to set the CH divider of the OUT12 to 1250, this 12bit data will be stored in R1225[3:0] and R1226[7:0], but only R1226 can be written to the EEPROM, which means that I lost the higher 4 bits of the CH divider , and the result is that the output frequency of the OUT12 is incorrect after LMK5B33414EVM POR, the effective part is only the lower 8 bits of 1250.
After testing, it seems that all CH dividers of all output channels have the same bug, i.e. all OUT_x_y_CH_DIV_11: 8 can't load data from the EEPROM at POR, and you can see from the REGCOMMIT sequence that they have been lost.
This is causing us a lot of trouble as 0.5M is our planned power clock and we need it to be valid by default, could you please help to see if there is a way to fix it?