Part Number: LMX2595
Tool/software:
Hi:
As shown in the figure below, if I want multiple LMX2595 chip outputs with the same configuration to be synchronized, which SYNC Category should be selected?
OSCin = 200MHz
PFD = 200MHz
VCO = 9600MHz
Fout = 1600MHz
Since the minimum value of N DIVIDER is 28, we need to set VCO_PHASE_SYNC = 0.
I checked the manual Figure 33. Determining the SYNC Category, but did not find a suitable synchronization mode.
Thank you!