Part Number: LMKDB1108
Tool/software:
Hello,
I have a design using the LMKDB108Z100RKPT and I cannot get the LOS# on pin 1 to go low when I remove the Clock Input.
Here is the setup:
1) VDDA is at 3.3V,
2) The PWRGD/PWRDN# (pin 12) is at 3.3V,
3) The SLEWRATE_SEL is pulled to 3.3V through 4.75K resistor.
4) The OE# (Output Enable) for CLK0, CLK1, CLK2, and CLK3 on pins 14, 19,21, and 27 are all pulled low.
5) The Output Enable bits in Reg0 and Reg1 for CLK0, CLK1, CLK2, and CLK3 are programmed high.
5) The LOS# on pin 1 is pulled up to 3.3V through a 4.75K ohm resistor.
I provide an a differential input clock that is close to 1400mVp-p on the CLKIN_P (pin 8) and CLKIN_N(pin 9) inputs. The clock outputs of the LMKDB1108 show 1300mVp--p differential clocks on CLK0, CLK1, CLK2 and CLK3 pins. The LOS# (Pin 1) is high (pulled to 3.3V through a 4.75K ohm resistor). I remove the differential Clock input and let the Clock_P and CLOCK_N inputs just float (They each have a 750mV DC bias). When I remove the differential Clock Input, all the output clocks stop. I expected the LOS# on pin 1 to go low, however, it remained at 3.3V (Through the 4.75K ohm pull-up to 3.3V). Any help would be appreciated. Thanks in advance.