This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM567C: SNR Level detection needed (?)

Part Number: LM567C

Tool/software:

Hi

What should be the minimum Signal-to-Noise Ratio (SNR) for possible detection? (If the signal is buried in noise, is it still possible to detect it?).

I understand that the SNR at the input must be improved as much as possible, but I don't know by how much.

My conditions ;

V power = 5V

Input signal > 200mV rms, F0= 300KHz square, Burst = 60 x pulses répétitive  +white noise broadband (Level ? )

Not easy to understand your datasheet "Minimum Input Signal to Wideband Noise Ratio" Bn = 140 kHz

Best regards.