Part Number: LMX2594
Tool/software:
Hello! There are several questions regarding the use of LMX2594 as follows:
1.If for the RF output port, I only use one RFOUTAP, and the remaining three RFOUTAM, RFOUTBM, and RFOUTBP are directly grounded at 50 ohms?

2. Is the LO output power given in the manual single-channel power or differential power?

3. Can the power supply of VCCBUF be provided together with the other several lines? (If differential output is not adopted)