Part Number: CDCE6214
Tool/software:
So I'm reading:
"By factory default, the page 0 EEPROM has pin mode enabled, meaning that the 4 GPIO pins are configured as individual OE pins.
R0[0] defines the pin mode, but this bit will only take effect when written to EEPROM"
If I want to select Serial Interface Mode (not fall back mode) at power on what voltage level do I set REFSEL and HW_SW_CTRL to? (the table shows L/H probably due to the EEPROM page number, but I don’t see how to differentiate between pin mode and serial interface mode at power up)
I think I would need to program EEPROM's R0[0] but I'm confused. Thanks!