This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE906: Creating config file for CDCE906

Part Number: CDCE906

Tool/software:

Hi, I am trying to create a config file for the CDCE906 chip using  TI Pro Clock's Programming Assistant. I need to set specific values for the divider and multiplier, but it only allows me to set the input and output frequencies. My input is a variable differential input with a range of 20-40kHz and I need to have specific values for multiplier and divider to have variable output at the end with respect to the variable input. I was wondering if you would know how to resolve the problem.  I have the CDCEx06 Programming EVM working, I just need to create a config file to program the chip. 

I also wanted to confirm whether I placed the CDCE906 chip correctly, because the schematic in the manual was a bit different from the one on board.

Thank you, 

Best Regards, 

Disha