Other Parts Discussed in Thread: CDCE62005
We have built a PCB using the CDCE62005 and facing three problems.
The usage scenario is rather simple. There are two clock sources, both 40 MHz. The primary section is connected to a connector, and the secondary side is driven by a local oscillator. If there is no primary input, the CDCE62005 planned to switch to the “backup” secondary (oscillator input). All outputs are used, some of those in LVDS some in CMOS mode.
We have designed a CDCE62005 firmware download tool that reads the output file of the CDCE62005 GUI, makes programming, EEPROM refresh (if needed), calibrates and check for lock status.
We have 3 problems:
1, At a first stage of the bring up, we have faced the following problem. (The chip is running fixed from onboard oscillator, CMOS input used). Everything is fine all frequencies (25, 64, 96 MHz) are good, lock is ok, BUT on the output 0 there is no clock !!! Used in LVDS mode. All the other outputs are working fine, we can output the same frequency to other outputs, but 0 is not working …. (This problem was temporary solved with a bypass wire.)
We have checked the issue on multiple PCBs !?
2, At the final application the clock input standard will be LVDS. So we have reconfigured the secondary input to LVDS. (oscillator + LVDS driver DS90LV011). We do not get lock ! And if we configure one output to be directly connected to the input, nothing is there. We tried many configuration, and found out that turning “Fail safe” off, solves the issue …We tried all combination of internal/external AC/DC. None is working, while the failsafe is on.
OK. We can
live with this somehow.
3, BUT! We can not get the primary input into lock in LVDS mode. The CMOS mode is ok. LVDS AC/DC/Failsafe on/off is not locking in any combination, though direct routing to the primary input to one of the output is ok. I think the smart mux can not detect the valid source, that is why it is not enabling the PLL at all, or something like this…. (It is crazy because the same source connected to the secondary input works really nince, when failsafe is off!!!! )
Do you have any idea???
PCB is ok I think, we have good decoupling + supply filtering and dedicated LDO for the CDCE62005.