Part Number: CDCM6208
Tool/software:
Dear Experts
At present, the existing products are experiencing equipment failures in end customers. After investigation, we found that it is caused by abnormal IIC configuration of CDCM6208.
The specific reason is that CDCM6208 did not return ACK normally, resulting in MCU IIC bus hanging up, failure to complete CDCM6208 register configuration, abnormal clock output, and device function abnormalities; We have tried to modify the 4.7K Ω pull-up resistor to 1K Ω pull-up resistor, and the fault has been optimized.
We have compared the signal quality and timing of the two pull-up resistors, and both meet the requirements of the data manual. Currently, it is unclear the specific cause of the IIC fault. Does the chip have strict requirements for the rising edge slope or high-level cycle? What is the minimum IIC pull-up resistor that CDCM6208 can use?