Tool/software:
Hi TI forum,
I'm new with this devices and I'm currently trying to configure the 'tutorials' inside User's Guide. When setting up FSK mode same way as UG and using a waveform generator with square waveform and 1 Vpp with a frequency of 20 kHz on MOD Test Point, and I can't recognise any difference in the output with the trigger on or off in Vtune test point.
(The difference you see at the corner is noise)
Also, when configuring trapezoid I found out it may have problems with ramp down because it can generate it
I tried a different test looking for ramp down I got the same, just a constant voltage and abrumpt jump in voltage
I can't find anything in the UG or my setup.
I can share more info if needed, such as pictures on how everything is connected.
Thanks in advance,
Joaquín.