Part Number: LMX2820
Tool/software:
Hi Team. I am currently working with two LMX2820 PLLs in my application, both driven by the same 100 MHz reference clock. One PLL is configured to generate variable frequency ranging from 7 to 14 GHz with 25 MHz steps, while the other is set to a fixed output frequency of 9 GHz. My objective is to achieve phase synchronization between these two PLLs. Could you please provide guidance on utilizing the PSYNC functionality to accomplish this? I have tied two PYNSC signals of PLL1 and PLL2 in this scenario.
Thankyou.