Tool/software:
Hello, could you please take a look at this design based on the TPL5110 that I created using the various recommendations you provided? The goal is to make a timing circuit for a 24V relay with a contact current of 1A and a coil current of 4.6mA. The aim is to set this time between 0 and 10 minutes using the different values given in the component datasheet. The time should only be changed when the power is turned off; for example, to switch from 1 minute to 2 minutes, we turn off the power. The coil contact is initially open, and once the coil is powered, this contact closes and only opens when the power is cut and the defined time has elapsed. Thank you in advance for your help