Part Number: CDCE6214Q1TM
Other Parts Discussed in Thread: CDC6C, LMK00334, , SN74LVC2G17, DS90LV028A, SN65LVDS2, DS90LV018A, DS90LV017A, CDCE6214-Q1, DS90LV001, ADS1299
Tool/software:
Hi Team,
I was planning to use clock generator for my application which requires at least 2 outputs with one frequency fixed at 2.048MHz going to ADS and another may vary from 2-8 MHz going to MCU, the input is from a crystal with either 12.288MHz or 25MHz (any one based on feasibility).
The clock signal trace will be running to multiple boards on the back plane and the trace length ~400mm max from end to end.
My concerns with the clock generator are:
1. Is it okay to use single ended clock signal from EMI/EMC point of view?
2. If I am going with single ended signal, is the drive strength of the clock generator is good enough or do I need a buffer at the driver side?
3. If I am going with LVDS signal, is the drive strength of the clock generator is good enough or do I need a LVDS buffer at the driver side and can you suggest some LVDS to Single ended 2:2 converters for the receiver side?
4. There is an high possibility that I might use different clock generator with single ended output. If LVDS is strongly recommended, can you suggest some single ended to LVDS converter?
Thank you