This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832EVM-CVAL: Register space address size confirmation

Part Number: LMK04832EVM-CVAL
Other Parts Discussed in Thread: LMK04832

Tool/software:

Hello! The LMK04832 Datasheet claims "15-bit address field (A14 to A0) and a 8-bit data field (D7 to D0)" (section 8.5), but the registers listed only span 0x000 to 0x555, which only utilizes 11 bits. Could TI please confirm that there is not actual data beyond register 0x555? Our architecture may limit the number of available address bits, and I would like to confirm that I'm not causing myself to not have the ability to read some "hidden" debug registers that we may need further down the road.

Thank you!

Eric M.