Part Number: LMK01010
Other Parts Discussed in Thread: LMK01801, LMK01000
Tool/software:
I am planning to use differential input clock and differential output clock.
The clock of each output channel should have a delay control function for timing control.
The clock of the output channel does not have divide and only uses the delay function.
That is, the input clock and the output clock have the same frequency.
The material I found at TI is LMK01010.
1. Please recommend an IC among the clock buffers that can control the output channel delay.
2. If I use the delay function for the output channel without using sync and without divide in LMK01010, will the clocks of the output channels be synchronized to the input clock and output with a delay of the set delay value?
3. Even if the frequencies of the input clock and the output clock are the same, should I use the sync function when using the delay function for the output channel?